Raritan EMX JSON-RPC API
LuaService.idl
1 /* SPDX-License-Identifier: BSD-3-Clause */
2 /*
3  * Copyright 2015 Raritan Inc. All rights reserved.
4  */
5 
6 /**
7  * Lua-Service
8  *
9  * Lua-Service is a service that you can use to upload and execute a Lua script.
10  *
11  * When the service is starting, a cleanup will be happend at first. That means
12  * still running scripts will be killed and it will be tested for which script is
13  * an option given. Does here something not match, then the script or the option
14  * will be deleted.
15  *
16  * After the service is launched, the option 'autoRestart' will be for any script
17  * evaluated. If the flag is 'true', the script is going to be executed with a
18  * short delay (Environment->autoStartDelay).
19  *
20  * You can download and upload a script with the commands getScript() and setScript().
21  * When on uploading the script name is not present a new script will be created.
22  * If the name is already taken, then the old script will be overwritten.
23  *
24  * Use startScript() to execute a lua script and terminateScript() to stop a script.
25  * If the option 'autoRestart' is set to 'true', then the script starts automatically
26  * after it has exited.
27  *
28  * To get the output for a script use the command getScriptOutput(). The output
29  * is limited to 'Environment->outputBufferSize' bytes and mapped to a virtual
30  * address. On the first query call the method with starting address zero. After
31  * that use the returned address 'nAddr' for the next request.
32  *
33  * A script can be called with arguments (see options and startWithArgs).
34  */
35 module luaservice {
36 
37  /**
38  * A structure that descripts the state of a script.
39  *
40  * When a script is uploaded the new execState is STAT_NEW. exitCode and
41  * signal is not valid.
42  *
43  * When the execState is changing to STAT_TERMINATED then exitCode and signal
44  * will be set.
45  */
46  structure ScriptState {
47 
48  /** execution state for a scripts */
49  enumeration ExecState {
50  STAT_NEW, ///< the script never ran (after uploading or system (re)start)
51  STAT_RUNNING, ///< script state is running
52  STAT_TERMINATED, ///< script state is terminated
53  STAT_RESTARTING ///< script is terminated and restarts after 'restart interval'
54  };
55 
56  /** Descripts the type of exitStatus */
57  enumeration ExitType {
58  EXIT_CODE, ///< exitStatus is an exit code
59  SIGNAL ///< exitStatus is a signal
60  };
61 
62  ExecState execState; ///< execution state of the script
63  ExitType exitType; ///< type of exit code
64  int exitStatus; ///< exit status or signal
65  };
66 
67  /** some script options */
68  structure ScriptOptions_2_0_0 {
69  map <string, string> defaultArgs; ///< default arguments are passed to the lua script
70  boolean autoStart; ///< starts a script after system booting
71  boolean autoRestart; ///< restarts a script after termination or crash
72  };
73 
74  /**
75  * The struct represents two kinds of information:
76  * - limit (l)
77  * - current status (cs)
78  * Is a limit set to zero then there is no limit set. The unit of size
79  * is byte. The unit of interval is millisecond.
80  */
81  structure Environment_2_0_0 {
82  int maxScriptMemoryGrowth;///< maximum virtual memory growth per script (l)
83  int maxAmountOfScripts; ///< number of scripts that can be stored (l)
84  int amountOfScripts; ///< number of scripts that are stored (cs)
85  int maxScriptSize; ///< maximum size of a script file (l)
86  int maxAllScriptSize; ///< maximum size of all script files (l)
87  int allScriptSize; ///< size of all script files (cs)
88  int outputBufferSize; ///< output buffer size per script (l)
89  int restartInterval; ///< minimum delay to next (re)start (cs)
90  int autoStartDelay; ///< minimum delay to 'autoStart' a script
91  };
92 
93  /**
94  * There is a single manager instance.
95  */
96  interface Manager_2_0_1 {
97 
98  /** Error codes */
99  constant int NO_ERROR = 0; ///< no Error
100  constant int ERR_INVALID_NAME = 1; ///< script name is invalid
101  constant int ERR_NO_SUCH_SCRIPT = 2; ///< script name not found
102  constant int ERR_MAX_SCRIPT_NUMBERS_EXCEEDED = 3; ///< maximum amount of stored script files is reached
103  constant int ERR_MAX_SCRIPT_SIZE_EXCEEDED = 4; ///< maximum size of a script file is reached
104  constant int ERR_MAX_ALL_SCRIPT_SIZE_EXCEEDED = 5; ///< maximum size of all script files is reached
105  constant int ERR_NOT_TERMINATED = 6; ///< script is not terminated
106  constant int ERR_NOT_RUNNING = 7; ///< script is not running
107  constant int ERR_INVALID_ADDR = 8; ///< address parameter is wrong
108  constant int ERR_TOO_MANY_ARGUMENTS = 10; ///< too many arguments
109  constant int ERR_ARGUMENT_NOT_VALID = 11; ///< the argument has one or more invalid characters
110 
111  /**
112  * Upload a script to instance
113  *
114  * If there is a script with the same name the new script will replace
115  * the existing script (script must be in STAT_NEW or STAT_TERMINATED).
116  *
117  * @param name The name of the script file
118  * @param script The script file packed in a string
119  * @param options Options that can be set or not
120  *
121  * @return NO_ERROR if OK
122  * @return ERR_INVALID_NAME if script name is invalid
123  * @return ERR_MAX_SCRIPT_SIZE_EXCEEDED if the size of the new script is greater then the maximum file size
124  * @return ERR_MAX_ALL_SCRIPT_SIZE_EXCEEDED if maximum size of all script files is reached
125  * @return ERR_MAX_SCRIPT_NUMBERS_EXCEEDED if maximum amount of script files is reached
126  * @return ERR_NOT_TERMINATED if try to replace a running script
127  */
128  int setScript(in string name, in string script, in ScriptOptions_2_0_0 options);
129 
130  /**
131  * To download a script file to user.
132  *
133  * @param name The name of an existing script
134  *
135  * @return NO_ERROR if OK
136  * @return ERR_INVALID_NAME if script name is invalid
137  * @return ERR_NO_SUCH_SCRIPT if there is no script with the name
138  */
139  int getScript(in string name, out string script);
140 
141  /**
142  * Returns all script names in a string vector.
143  *
144  * If there are no scripts the vector is empty.
145  *
146  * @return A vector with all script names.
147  */
148  vector<string> getScriptNames();
149 
150  /**
151  * Deletes a script.
152  *
153  * @param name The name of the script
154  *
155  * @return NO_ERROR if OK
156  * @return ERR_INVALID_NAME if script name is invalid
157  * @return ERR_NO_SUCH_SCRIPT if there is no script with the name
158  * @return ERR_NOT_TERMINATED if try to delete a running script
159  */
160  int deleteScript(in string name);
161 
162  /**
163  * Sets new options for a script.
164  *
165  * @param name The name of the script
166  * @param options The new options
167  *
168  * @return NO_ERROR if OK
169  * @return ERR_INVALID_NAME if script name is invalid
170  * @return ERR_NO_SUCH_SCRIPT if there is no script with the name
171  * @return ERR_TOO_MANY_ARGUMENTS if the size of the map is to big
172  * @return ERR_ARGUMENT_NOT_VALID if a string in the arguments is not
173  */
174  int setScriptOptions(in string name, in ScriptOptions_2_0_0 options);
175 
176  /**
177  * Returns the options for a script.
178  *
179  * @param name The name of the script
180  * @param options The return value
181  *
182  * @return NO_ERROR if OK
183  * @return ERR_INVALID_NAME if script name is invalid
184  * @return ERR_NO_SUCH_SCRIPT if there is no script with the name
185  */
186  int getScriptOptions(in string name, out ScriptOptions_2_0_0 options);
187 
188  /**
189  * To query the environment information.
190  *
191  * @return a struct with the environment information
192  */
193  Environment_2_0_0 getEnvironment();
194 
195  /**
196  * To get output from a script as a string
197  *
198  * The output is stored in a string buffer with a defined size. The buffer is addressable with an
199  * (virtual) address. The address will be increased ervery time when the buffer will be filled.
200  *
201  * To get the output for the first time just call with address zero and then use the returned nAddr
202  * argument.
203  *
204  * If iAddr is negative then the last n bytes will be returned, e.g. -9 returns the last 9 characters.
205  * If iAddr is zero then the whole available buffer will be returned.
206  * If iAddr is positive then the returned buffer starts at this address.
207  * If iAddr is equal to nAddr then there is no data available
208  * If iAddr and oAddr is not equal then there were data lost (execption: first call with zero).
209  *
210  * @param name The name of the script
211  * @param iAddr The virtual start address where the returned output should begin.
212  * @param oAddr The virtual address from where the string starts.
213  * @param nAddr The virtual address for the next query.
214  * @param more A boolean whitch indicates if there is more data available.
215  *
216  * @return NO_ERROR if OK
217  * @return ERR_INVALID_NAME if file name is invalid
218  * @return ERR_NO_SUCH_SCRIPT if there is no script with the name
219  * @return ERR_INVALID_ADDR if iAddr is negative and the absolute value of parameter iAddr is greater as the limit
220  */
221  int getScriptOutput(in string name, in long iAddr, out long oAddr, out long nAddr, out string oString, out boolean more);
222 
223  /**
224  * Clear the output buffer of a script.
225  *
226  * @param name The name of the script
227  *
228  * @return NO_ERROR if OK
229  * @return ERR_INVALID_NAME if file name is invalid
230  * @return ERR_NO_SUCH_SCRIPT if there is no script with the name
231  */
232  int clearScriptOutput(in string name);
233 
234  /**
235  * To start a script
236  *
237  * The function starts a lua script.
238  *
239  * @return NO_ERROR if OK
240  * @return ERR_INVALID_NAME if file name is invalid
241  * @return ERR_NO_SUCH_SCRIPT if there is no script with the name
242  * @return ERR_NOT_TERMINATED if the script is running or restarting
243  */
244  int startScript(in string name);
245 
246  /**
247  * To start a script with arguments
248  *
249  * The function starts a lua script. Additionally you can add arguments which are available from the
250  * lua script. This args will override the default arguments. All args are stored in a global table
251  * called ARGS in lua.
252  *
253  * @return NO_ERROR if OK
254  * @return ERR_INVALID_NAME if file name is invalid
255  * @return ERR_NO_SUCH_SCRIPT if there is no script with the name
256  * @return ERR_NOT_TERMINATED if the script is running or restarting
257  * @return ERR_TOO_MANY_ARGUMENTS if the size of the map is to big
258  * @return ERR_ARGUMENT_NOT_VALID if a string in the arguments is not valid
259  */
260  int startScriptWithArgs(in string name, in map<string, string> arguments);
261 
262  /**
263  * To stop a script
264  *
265  * This command stops a running or restarting script. After terminating the option autorestart will
266  * not be evaluated.
267  *
268  * @return NO_ERROR if OK
269  * @return ERR_INVALID_NAME if file name is invalid
270  * @return ERR_NO_SUCH_SCRIPT if there is no script with the name
271  * @return ERR_NOT_RUNNING if the script is not running or restarting
272  */
273  int terminateScript(in string name);
274 
275  /**
276  * Returns the state for a single script.
277  *
278  * @param name The script name
279  * @param state The state of the script
280  *
281  * @return NO_ERROR if OK
282  * @return ERR_INVALID_NAME if file name is invalid
283  * @return ERR_NO_SUCH_SCRIPT if there is no script with the name
284  */
285  int getScriptState(in string name, out ScriptState state);
286 
287 
288  /**
289  * Returns the state for all scripts. If the map is empty then there are no scripts on the machine.
290  *
291  * @return A map<string name, ScriptState state> with name and state for all available scripts.
292  */
293  map<string, ScriptState> getScriptStates();
294  };
295 
296 }
int maxScriptMemoryGrowth
maximum virtual memory growth per script (l)
Definition: LuaService.idl:82
ExitType exitType
type of exit code
Definition: LuaService.idl:63
some script options
Definition: LuaService.idl:68
script state is terminated
Definition: LuaService.idl:52
int outputBufferSize
output buffer size per script (l)
Definition: LuaService.idl:88
the script never ran (after uploading or system (re)start)
Definition: LuaService.idl:50
int exitStatus
exit status or signal
Definition: LuaService.idl:64
There is a single manager instance.
Definition: LuaService.idl:96
int maxAllScriptSize
maximum size of all script files (l)
Definition: LuaService.idl:86
int maxScriptSize
maximum size of a script file (l)
Definition: LuaService.idl:85
A structure that descripts the state of a script.
Definition: LuaService.idl:46
ExecState execState
execution state of the script
Definition: LuaService.idl:62
int maxAmountOfScripts
number of scripts that can be stored (l)
Definition: LuaService.idl:83
The struct represents two kinds of information:
Definition: LuaService.idl:81
boolean autoStart
starts a script after system booting
Definition: LuaService.idl:70
Lua-Service.
Definition: LuaService.idl:35
exitStatus is an exit code
Definition: LuaService.idl:58
ExitType
Descripts the type of exitStatus.
Definition: LuaService.idl:57
int amountOfScripts
number of scripts that are stored (cs)
Definition: LuaService.idl:84
int autoStartDelay
minimum delay to &#39;autoStart&#39; a script
Definition: LuaService.idl:90
int restartInterval
minimum delay to next (re)start (cs)
Definition: LuaService.idl:89
ExecState
execution state for a scripts
Definition: LuaService.idl:49
script state is running
Definition: LuaService.idl:51
map< string, string > defaultArgs
default arguments are passed to the lua script
Definition: LuaService.idl:69
int allScriptSize
size of all script files (cs)
Definition: LuaService.idl:87
boolean autoRestart
restarts a script after termination or crash
Definition: LuaService.idl:71