1 #ifndef __PERIPHERAL_DEVICE_MANAGER_IDL__ 2 #define __PERIPHERAL_DEVICE_MANAGER_IDL__ 4 #include <PeripheralDeviceSlot.idl> 5 #include <PeripheralDevicePackage.idl> 6 #include <PortFuse.idl> 7 #include <NumericSensor.idl> 9 #include <UserEvent.idl> 17 constant
int ERR_INVALID_PARAMS = 1;
58 valueobject SettingsChangedEvent extends
event.UserEvent {
64 valueobject DeviceEvent_2_0_0 extends
idl.Event {
65 vector<Device_3_0_1> devices;
70 valueobject DeviceAddedEvent_2_0_0 extends DeviceEvent_2_0_0 { };
73 valueobject DeviceRemovedEvent_2_0_0 extends DeviceEvent_2_0_0 { };
76 valueobject UnknownDeviceAttachedEvent extends
idl.Event {
89 valueobject DeviceFirmwareUpdateStateChangedEvent extends
idl.Event {
100 valueobject FirmwareUpdateStateChangedEvent extends
idl.Event {
105 valueobject PackageEvent_2_0_0 extends
idl.Event {
106 vector<PackageInfo_2_0_1> packageInfos;
111 valueobject PackageAddedEvent_2_0_0 extends PackageEvent_2_0_0 { };
113 valueobject PackageRemovedEvent_2_0_0 extends PackageEvent_2_0_0 { };
125 vector<DeviceSlot_2_0_2> getDeviceSlots();
140 vector<Device_3_0_1> getDiscoveredDevices();
147 vector<PackageInfo_2_0_1> getDiscoveredPackageInfos();
164 int setSettings(in
Settings settings);
178 vector<DeviceTypeInfo> getDeviceTypeInfos();
200 vector<Package_1_0_1> getDiscoveredPackages();
int cSumErrCnt
CRC / checksum error counter.
Definition: PeripheralDeviceManager.idl:117
A sensor with numeric readings.
Definition: NumericSensor.idl:12
ZCoordMode zCoordMode
Z coordinate semantics.
Definition: PeripheralDeviceManager.idl:27
Range of possible sensor readings.
Definition: NumericSensor.idl:19
DeviceFirmwareUpdateState
Enumeration: State of device firmware update.
Definition: PeripheralDeviceManager.idl:82
peripheral DeviceManager's s settings
Definition: PeripheralDeviceManager.idl:26
ZCoordMode
Z Coordinate Mode identifier.
Definition: PeripheralDeviceManager.idl:20
int presenceDetectionTimeout
Timeout for presence detection (sec)
Definition: PeripheralDeviceManager.idl:30
Z coordinate of slot settings is in rack units.
Definition: PeripheralDeviceManager.idl:21
sensors::Sensor_4_0_2 TypeSpec type
Device (sensor) type.
Definition: PeripheralDeviceManager.idl:43
vector< PackageInfo_2_0_1 > allPackages
New list of discovered packages after change.
Definition: PeripheralDeviceManager.idl:107
Peripheral Devices.
Definition: PeripheralDeviceManager.idl:12
Peripheral Device Manager.
Definition: PeripheralDeviceManager.idl:15
Peripheral device statistics.
Definition: PeripheralDeviceManager.idl:116
Settings newSettings
Settings after change.
Definition: PeripheralDeviceManager.idl:60
Update has finished successfully.
Definition: PeripheralDeviceManager.idl:84
boolean isActuator
Is actuator or not.
Definition: PeripheralDeviceManager.idl:44
DeviceFirmwareUpdateState state
Update state.
Definition: PeripheralDeviceManager.idl:93
vector< Device_3_0_1 > allDevices
New list of discovered devices after change.
Definition: PeripheralDeviceManager.idl:66
boolean active
true if any peripheral device is currently updated
Definition: PeripheralDeviceManager.idl:53
int maxActivePoweredDryContacts
The maximum number of concurrently active powered dry contacts.
Definition: PeripheralDeviceManager.idl:32
vector< PosElement > position
Device position in the chain.
Definition: PeripheralDeviceManager.idl:78
Basic IDL definitions.
Definition: Event.idl:6
string serial
Serial number of device.
Definition: PeripheralDeviceManager.idl:92
Numeric sensor thresholds.
Definition: NumericSensor.idl:106
Firmware update status.
Definition: PeripheralDeviceManager.idl:52
Ports.
Definition: Port.idl:10
Update is running.
Definition: PeripheralDeviceManager.idl:83
string identifier
Device type identifier.
Definition: PeripheralDeviceManager.idl:45
string name
Device type display name.
Definition: PeripheralDeviceManager.idl:46
Sensor interface
Definition: Sensor.idl:10
Sensors Model.
Definition: AccumulatingNumericSensor.idl:8
int remaining
Number of peripheral devices that are still pending to be updated.
Definition: PeripheralDeviceManager.idl:54
Interface describing a controllable fuse for a device port.
Definition: PortFuse.idl:12
string newVersion
Firmware version to be updated to.
Definition: PeripheralDeviceManager.idl:91
Peripheral Device Slot.
Definition: PeripheralDeviceSlot.idl:55
boolean autoManageNewDevices
Automatically manage newly detected devices.
Definition: PeripheralDeviceManager.idl:28
float deviceAltitude
Altitude of device in meters.
Definition: PeripheralDeviceManager.idl:29
sensors::NumericSensor_4_0_2 Range defaultRange
Default sensor range (numeric sensors only)
Definition: PeripheralDeviceManager.idl:47
Complete sensor type specification.
Definition: Sensor.idl:153
int defaultDecDigits
Default sensor precision (numeric sensors only)
Definition: PeripheralDeviceManager.idl:48
Peripheral device type info.
Definition: PeripheralDeviceManager.idl:42
map< string, sensors::NumericSensor_4_0_2.Thresholds > defaultThresholdsMap
Default thresholds by peripheral device type.
Definition: PeripheralDeviceManager.idl:31