Raritan PX2/PX3 JSON-RPC API
Classes | Public Member Functions | Public Attributes | List of all members
lhxmodel::Lhx_3_2_5 Interface Reference

LHX Interface. More...

import"Lhx.idl";

Classes

struct  AlertStatus
 LHX alert status. More...
 
struct  Capabilities
 LHX capabilities. More...
 
struct  MetaData
 LHX metadata. More...
 
struct  OpState
 LHX operational state. More...
 
struct  ParamCfg
 Configuration parameter characteristics. More...
 
struct  Settings
 LHX settings. More...
 

Public Member Functions

Capabilities getCapabilities ()
 Retrieve the LHX capabilities (static).
 
MetaData getMetaData ()
 Retrieve the LHX metadata. More...
 
Settings getSettings ()
 Retrieve the LHX settings. More...
 
int setSettings (in Settings settings)
 Change the LHX settings. More...
 
vector< Sensor_4_0_4getSensors ()
 Get LHX sensors.
 
OpState getOpState ()
 Get LHX operational state.
 
int setPowerState (in sensors::Sensor_4_0_4.OnOffState state)
 Switch powerstate of LHX. More...
 
vector< Parameter_2_0_1getParameters ()
 Get parameter list.
 
vector< Parameter_2_0_1getActualValues ()
 Get actual value list.
 
int setMaximumCoolingRequest (in boolean requested)
 Request maximum cooling. More...
 
int acknowledgeAlertStatus ()
 Acknowledge alert status. More...
 

Public Attributes

constant int ERR_INVALID_PARAMS = 1
 Invalid parameters.
 
constant int ERR_NOT_SUPPORTED = 2
 Not supported.
 
valueobject OpStateChangedEvent: idl::Event { OpState oldState
 Event: LHX operational status has changed. More...
 
OpState newState
 Status after change.
 
valueobject SettingsChangedEvent: event::UserEvent { Settings oldSettings
 Event: LHX settings have changed. More...
 
Settings newSettings
 Settings after change.
 

Detailed Description

LHX Interface.

Member Function Documentation

◆ acknowledgeAlertStatus()

int lhxmodel::Lhx_3_2_5::acknowledgeAlertStatus ( )

Acknowledge alert status.

Returns
0 if OK
ERR_NOT_SUPPORTED if operation is not supported

◆ getMetaData()

MetaData lhxmodel::Lhx_3_2_5::getMetaData ( )

Retrieve the LHX metadata.

Returns
LHX metadata

◆ getSettings()

Settings lhxmodel::Lhx_3_2_5::getSettings ( )

Retrieve the LHX settings.

Returns
LHX settings

◆ setMaximumCoolingRequest()

int lhxmodel::Lhx_3_2_5::setMaximumCoolingRequest ( in boolean  requested)

Request maximum cooling.

Parameters
requestedtrue if request maximum cooling false if request normal operation
Returns
0 if OK
ERR_NOT_SUPPORTED if operation is not supported

◆ setPowerState()

int lhxmodel::Lhx_3_2_5::setPowerState ( in sensors::Sensor_4_0_4.OnOffState  state)

Switch powerstate of LHX.

Parameters
stateon or off
Returns
0 if OK
ERR_NOT_SUPPORTED if operation is not supported

◆ setSettings()

int lhxmodel::Lhx_3_2_5::setSettings ( in Settings  settings)

Change the LHX settings.

Parameters
settingsNew LHX settings
Returns
0 if OK
ERR_INVALID_PARAMS if any parameters are invalid

Member Data Documentation

◆ OpStateChangedEvent

valueobject lhxmodel::Lhx_3_2_5::OpStateChangedEvent

Event: LHX operational status has changed.

Status before change

◆ SettingsChangedEvent

valueobject lhxmodel::Lhx_3_2_5::SettingsChangedEvent

Event: LHX settings have changed.

Settings before change


The documentation for this interface was generated from the following file: